• No : 23304
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

What are the minimum applicable voltage and current of SR-T* andSRD-T* type contacts?
Category : 

Answer

The minimum applicable load is 20V, 3mA . Contact reliability is indicatedby fault rate λ60 (Number of fault / Operating cycles per one contact) atthe reliability level 60%. = 1*10-7 / time
Product Name
Motor Starters
Series
MS-T/N