• No : 23312
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

Is it possible to install MS-T and MS-N series magnetic starter on thefloor?
Category : 

Answer

It is not possible to install it on the floor. If doing that, the weight of themoving part of a magnetic starter itself acts downward against thetripping spring, the shock at making time increases and the durabilitydecreases. Moreover, the operation when breaking may be late and thebreaking performance will be worse. If foreign materials such as dust stickto the contact, the contact reliability will be also worse.
Product Name
Motor Starters
Series
MS-T/N