• No : 23376
  • Release Date : 2018/09/12 15:12
  • Print

About Low-voltage Power Distribution Products

What is the purpose of individual control product of US-H*DD type?
Category : 

Answer

It is a product that can control two main circuit elements independently,and can be downsized when two or more single-pole type SSCs are used.It is also effective for controlling constant temperature extensively withmultiple single-phase heaters.
Product Name
Motor Starters
Series
MS-T/N