FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
Differences in the panel cutting dimensions from the GOT1000 series
Back
No : 23421
Release Date : 2018/09/14 15:06
Update : 2018/09/26 16:37
Print
Differences in the panel cutting dimensions from the GOT1000 series
Do the GOT1000 series and GOT2000 series have the same panel cutting dimensions when their models are the same in screen sizes?
Category :
FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT27
FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT25
FAQ
>
Human Machine Interfaces
>
Human-Machine Interfaces(HMIs)-GOT
>
GOT2000 Series
>
GT21
Answer
The GOT1000 series and GOT2000 series have the same panel cutting dimensions when their models are the same in screen sizes (excluding the GT25 open frame model).
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT
Series
GOT2000 Series