• No : 23422
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:38
  • Print

Compatibility of communication cables for the GOT1000 series

Answer

Only when the connectors have the same number of pins, shape, and communication format, the communication cable for the GOT1000 series can be used for the GOT2000 series as well.

The following communication cables for the GOT1000 series cannot be used for the GOT2000 series.
■ For GT16
  ・ GT16-C02RS-9S
  ・ GT16-C02RS-25S
  ・ FA-LTBGTR4CBL05
  ・ FA-LTBGTR4CBL10
  ・ FA-LTBGTR4CBL20
■ For GT10
  ・ GT10-RS2TUSB-5S
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Cable
Series
GOT2000 Series