• No : 23432
  • Release Date : 2018/09/14 15:06
  • Update : 2020/01/07 15:43
  • Print

Remote personal computer operation function (Ethernet)

Can the remote personal computer operation function (Ethernet) be used in the GOT2000 series?
Category : 

Answer

The remote personal computer operation function (Ethernet) can be used in the GOT2000 series as well.

Note the following when using the function.
1. The remote personal computer operation function (Ethernet) license for the GOT2000 Series (GT25-PCRAKEY) is required.
2. For GT Designer3 Version1.185T or later and earlier than Version1.225K,
  set "GOT Graphic Ver.1" to the graphics setting. If "GOT Graphic Ver.2" is set,
  a message appears saying "This function cannot be used" when GOT calls the
  remote personal computer operation function (Ethernet).
  Note that "GOT Graphic Ver.2" can be used with GT Designer3 Version1.225K or later.

  For the details of the graphics setting, refer to the following manual.
  GT Designer3 (GOT2000) Screen Design Manual (SH-081220-AC)
  "5.1.5 [Type Setting] dialog ■1 [Basic Setting]"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Supported model (remote personal computer operation function (Ethernet)), license (remote personal computer operation function (Ethernet))
Series
GOT2000 Series