• No : 23434
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:48
  • Print

MES interface function

Can the MES interface function be used in the GOT2000 series?
Category : 

Answer

◆ For GT Designer3 (GOT2000) Version1.108N or later
The MES interface function can be used in the GOT2000 series as well.

However, the license of the MES interface function for the GOT2000 series (GT25-MESIFKEY) is required.
In addition, when the BootOS version of the GOT is "C" or earlier, updating the BootOS version to "D" or later is required.

* To update the BootOS version to "D" or later, GT Designer3 (GOT2000) Version1.108N or later is required.

For information on how to update (install) the BootOS, refer to the following.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG)
 "4.4.3 Transferring data" or
 "4.5.3 Installing the BootOS or the CoreOS to the GOT"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Supported model (MES interface)
Series
GOT2000 Series