FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
Using with the GOT1000 series in the client/server function
Back
No : 23435
Release Date : 2018/09/14 15:06
Update : 2018/09/26 16:49
Print
Using with the GOT1000 series in the client/server function
Can a GOT1000 series model and a GOT2000 series model be used together on a client/server of the gateway function?
Category :
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
GT27
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
GT25
Answer
A GOT1000 series model and a GOT2000 series model can be used together on a client/server of the gateway function.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gateway)
Series
GOT2000 Series