• No : 23438
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:52
  • Print

Wireless LAN communication unit and wireless LAN access point

Answer

The wireless LAN communication unit (GT25-WLAN) can be used as an access point.

* Compatible with GT Designer3 (GOT2000) Version1.144A or later.
 Use the BootOS version "C" or later.

* Up to five stations are connectable.

* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
 For the details, refer to the following Technical News.
・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Communication unit
Series
GOT2000 Series