FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
Connecting FA devices through the wireless LAN communication unit (GT25-WLAN)
Back
No : 23439
Release Date : 2018/09/14 15:06
Update : 2018/09/26 16:53
Print
Connecting FA devices through the wireless LAN communication unit (GT25-WLAN)
Can an FA device such as a PLC and the GOT be connected through a wireless LAN by using the wireless LAN communication unit (GT25-WLAN)?
Category :
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
GT27
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
GT25
Answer
An FA device such as a PLC and the GOT cannot be connected through a wireless LAN by using the wireless LAN communication unit (GT25-WLAN).
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Communication unit, GOT function (communication)
Series
GOT2000 Series