• No : 23455
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 20:53
  • Print

Gesture functions available for the alarm display

Answer

The following gestures are available for the alarm list display.

◆ GT Designer3 (GOT2000) Version 1.100E or later
・ Tap: Displays the cursor on the tapped row.
・ Tap on the cursor row: Switches between the detail display and hierarchy display (equivalent to the key code switch FFB8).  
・ Double-tap: Switches the double-tapped row between the detail display and hierarchy display.
・ Swipe along the time axis: Scrolls the alarm list display by half the page in the swiped direction.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), GOT function (alarm)
Series
GOT2000 Series