Perform the following procedure to use the screen gesture function. 
The screen gesture function is only available for the GOT3000 series (models with a capacitive-type touch panel) and GT27 models.
◆ For GT Designer3 (GOT2000) Version 1
1. Select [Common] → [GOT Type Setting] then select [Use the gesture function] and click [OK]. 
2. Place a key code switch (screen gesture mode switching) to switch between screen gesture mode and normal operation mode in the screen gesture inactive area (a 32-dot area from the top of the screen) on the base screen. 
3. Touch the key code switch (screen gesture mode switching) placed on the base screen of the GOT.
To display the screen gesture inactive area on the drawing screen, select [Screen] → [Screen Property]. Then select [Display the screen gesture inactive area] and click [OK].
For the GT27 model, in addition to the settings above, select [Common] → [GOT Type Setting] then select [Enable the graphics accelerator] to smooth the drawing process. 
This setting is available under the following conditions. 
GT Designer3 (GOT2000) Version 1.185T or later with GOT Graphic Ver.1, or
GT Designer3 (GOT2000) Version 1.112S or later but 1.181P or earlier
However, the following restrictions apply. 
 • GOT startup may become slower. 
 • The displayed objects will not be refreshed in screen gesture mode.