• No : 23469
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 18:11
  • Print

Refreshing the monitor screen in screen gesture mode

Answer

The monitor screen may or may not be refreshed in screen gesture mode as listed in the table below.

1. GT37 model
The monitor screen refreshes. 
* For the GT37 models, only models that have a capacitive-touch panel are compatible with screen gesture mode. 
2. GT27 model
As shown in the following table. 

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series, GOT3000 Series