- No : 23478
- Release Date : 2018/09/14 15:06
-
Print
System dialog display in the screen gesture mode
What operation is performed when the system dialog is displayed in the screen gesture mode?
- Category :
-
Answer
When the system dialog is displayed in the screen gesture mode, enlargement or scrolling is canceled and the screen display returns to the normal size (100%).
Also, the screen gesture mode is canceled.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (standard function)
- Series
- GOT2000 Series