What happens when the system dialog is displayed in screen gesture mode?
When the system dialog is displayed in screen gesture mode, zooming and scrolling are disabled and the screen returns to the original size (100%). Screen gesture mode is disabled.
* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.