• No : 23481
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 18:09
  • Print

Touching the screen gesture active area

How can I touch the switches placed in the screen gesture active area in the screen gesture mode?
Category : 

Answer

You cannot touch the switches in the screen gesture active area in the screen gesture mode.
To be able to touch the switches, touch either of the following switches placed outside the screen gesture active area to cancel the screen gesture mode.

・ Screen gesture mode selector switch (key code: FF90)
・ Full scale display (100%) switch (key code: FF91)

* The full scale display (100%) switch is supported by GT Designer3 (GOT2000) Version 1.105K or later.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series