◆ GT Designer3 (GOT2000) Version 1.105K or later
When the screen gesture mode is enabled, a frame indicating the screen gesture active area is displayed.
This frame consists of a bright red line only when the display contents inside the screen gesture active area are not enlarged, and a bright red line and dark red line when the display contents are enlarged. The length and position of the bright red line of the frame indicate where the enlarged display area corresponds the range in the full scale (100%) screen.