• No : 23497
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/16 16:09
  • Print

Transferring data between a personal computer and a GOT via a PLC

Answer

The GOT screen data can be read and written from and to a personal computer via a PLC.

Note that the following items have restrictions. 
• Connection type between the personal computer and the PLC
• Connection type between the PLC and the GOT
• Relay PLC type
• Screen design software version

The following items have restrictions depending on the relay PLC type.
• Serial number of the PLC
• PLC engineering software version

For details, refer to the screen design software manual. 

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (screen data transfer)
Series
GOT3000 Series, GOT2000 Series