FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
Vertical installation of the rugged model
Back
No : 23518
Release Date : 2018/09/14 15:07
Update : 2018/09/26 15:22
Print
Vertical installation of the rugged model
Can the rugged model be used vertically?
Category :
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
GT25
FAQ
>
Human Machine Interfaces
>
Human Machine Interfaces MELHMI-GOT
>
GOT2000 Series
>
GT25 Rugged
Answer
The rugged model can be used vertically.
An arrow instructing the vertical installation is shown on the back of the GOT. Install the GOT vertically in the direction of the arrow.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model
Series
GOT2000 Series