• No : 23518
  • Release Date : 2018/09/14 15:07
  • Update : 2018/09/26 15:22
  • Print

Vertical installation of the rugged model

Answer

The rugged model can be used vertically.
An arrow instructing the vertical installation is shown on the back of the GOT. Install the GOT vertically in the direction of the arrow.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model
Series
GOT2000 Series