- No : 23542
- Release Date : 2018/09/14 15:07
-
Print
Location of the terminating resistor setting switch for the RS-422/485 communication port
Where is the terminating resistor setting switch for the RS-422/485 communication port located on the rugged model?
- Category :
-
Answer
The terminating resistor setting switch for the RS-422/485 communication port is located inside the battery cover on the back of the rugged model.
For the details, refer to the following.
GOT2000 Series User's Manual (Hardware) (SH(NA)-081194ENG-X)
"4.3 GT2507T-W"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series