• No : 23542
  • Release Date : 2018/09/14 15:07
  • Print

Location of the terminating resistor setting switch for the RS-422/485 communication port

Where is the terminating resistor setting switch for the RS-422/485 communication port located on the rugged model?
Category : 

Answer

The terminating resistor setting switch for the RS-422/485 communication port is located inside the battery cover on the back of the rugged model.

For the details, refer to the following.
GOT2000 Series User's Manual (Hardware) (SH(NA)-081194ENG-X)
"4.3 GT2507T-W"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model
Series
GOT2000 Series