- No : 23546
- Release Date : 2018/09/14 15:07
-
Print
Improved UV resistance of the rugged model
How has the UV resistance of the rugged model been improved?
- Category :
-
Answer
The UV resistance of the rugged model has been improved in two points.
The UV cutoff environmental protection sheet (not replaceable) is used on the GOT front face.
This reduces degradation of the touch panel and display.
Changing the material of the GOT front face from resin to aluminum reduces degradation of the front panel.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series