- No : 23714
- Release Date : 2018/09/19 17:16
-
Print
Position of switch
The memory of the settling switch for definite time current and instantaneous current has a prohibition position. If this position is selected, how does the relay operate?
- Category :
-
Answer
The prohibition position sets the maximum settling value. With the definite time current, all prohibition positions set 6 A, and with the instantaneous current, all prohibition positions set 60 A.
- Product Name
- Protection Relay
- Series
- MELPRO-A Series