• No : 23714
  • Release Date : 2018/09/19 17:16
  • Print

Position of switch

The memory of the settling switch for definite time current and instantaneous current has a prohibition position. If this position is selected, how does the relay operate?
Category : 

Answer

The prohibition position sets the maximum settling value. With the definite time current, all prohibition positions set 6 A, and with the instantaneous current, all prohibition positions set 60 A.
Product Name
Protection Relay
Series
MELPRO-A Series