• No : 24812
  • Release Date : 2019/04/09 15:18
  • Print

degrees of protection to  IEC60529

What is degrees of protection for MCCB, ELCB, ACB according to IEC60529?
Category : 

Answer

The degess of protection for ACB is IP20 as standard (under the condition that front door is closed). For MCCB and ELCB, the degrees of protection can be IP20 with terminal cover as seen from front-side. Refer to the figure as below.
 
Product Name
Molded Case Circuit Breakers
Series
WS-V