FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Pulse output type of the FX3U-1PG pulse output block
Back
No : 24972
Release Date : 2019/04/23 07:19
Print
Pulse output type of the FX3U-1PG pulse output block
What is the pulse output type of the FX3U-1PG?
Category :
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
FAQ
>
Controllers
>
Programmable Controllers MELSEC
>
MELSEC-F Series
>
Positioning Control
Answer
It is transistor output.
Transistor output specifications are as follows.
・ Rated load voltage 5 to 24 V DC
・ Maximum load current 20 mA or lower
Product Name
MELSEC-F Series
Product Category
FX3U,FX3UC
Series
Positioning Control