• No : 25010
  • Release Date : 2019/04/23 11:12
  • Print

Connection of a totem pole output encoder

Is it possible to connect a totem pole output encoder to the FX2NC-1HC/ FX2N-1HC/ FX3U-2HC high-speed counters?
Category : 

Answer

The totem pole output encoder cannot be connected to the FX2NC-1HC/ FX2N-1HC/ FX3U-2HC.
The connectable encoders are as follows.
・ Open collector output type encoder ∙ Differential line driver output type encoder
Product Name
MELSEC-F Series
Product Category
FX2N, FX2NC, FX3U
Series
High-Speed Counting