(1) When "N" is marked on the breaker,connect the N phase wire as marked.
(2) When "N" is not marked on the breaker, N phase wire can be connected to either pole (left or right).
* For 2-pole products with a 3-pole external shape, connect to the left and right poles without using the center pole.