What type of product is GT Works3?
GT Works3 is screen design software for the GOT3000, GOT2000, and GOT1000 series, integrating functions inspired by a user-oriented perspective under the three themes of simplicity, tidiness, and ease of use.
GT Works3 includes the following software products.
• GT Designer3, GT Simulator3
• GT SoftGOT3000
• Data Transfer Tool
etc.
* GT Simulator3 is installed when GT Designer3 is installed.
For details on the GT Works3 lineup and licenses, refer to the following.
[FAQ][GT Works3 product configuration]