- No : 20857
- Release Date : 2018/08/22 16:24
-
Print
CC-Link IE Field Basic
When CC-Link IE Field Basic is used, how many FR-A800-E or FR-F800-E can be connected at the maximum?
- Category :
-
Answer
Up to 64 (slave stations). The number of connectable units differs depending on the master station.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-E, FR-F800-E