• No : 20905
  • Release Date : 2018/08/22 16:25
  • Print

Frequency search

When the frequency search is performed by the combination with the general-purpose motor, how many Hz or lower is regarded as 0 Hz?
Category : 

Answer

DC application method (Pr.162 = 0 or 10): 4 Hz or lower is regarded as 0 Hz. AC application method (Pr.162 = 3 or 13): It is not defined since it depends on the electrical characteristic of the motor.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800