• No : 20907
  • Release Date : 2018/08/22 16:25
  • Print

PLC function

On what condition does the PLC function device: SM1217 turn ON?
Category : 

Answer

Vector control: The SM1217 turns ON when the motor rotates even if no forward rotation command is send. Other than vector control: The SM1217 turn ON by forward rotation + RUN (output frequency).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800