- No : 20971
- Release Date : 2018/08/22 16:25
-
Print
FR Configurator2 (trial version)
When I set the inverter model and click OK, an error of the error code: C.000000.5 Error during application execution occurs. What are the causes and countermeasures?
- Category :
-
Answer
The error may occur if the old version of GX-WORKS3 is used. Update GX-WORKS3 to the latest version.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Engineering software
- Series
- FR Configurator2