• No : 20971
  • Release Date : 2018/08/22 16:25
  • Print

FR Configurator2 (trial version)

When I set the inverter model and click OK, an error of the error code: C.000000.5 Error during application execution occurs. What are the causes and countermeasures?
Category : 

Answer

The error may occur if the old version of GX-WORKS3 is used. Update GX-WORKS3 to the latest version.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
FR Configurator2