- No : 20976
- Release Date : 2018/08/22 16:25
-
Print
FR-A800
When Pr.820: Speed control P gain 1 is set to 0%, how does it affect the response?
- Category :
-
Answer
Since the lower limit has been internally set, the setting value of 3 % or less is recognized as 3%.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800