• No : 20976
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800

When Pr.820: Speed control P gain 1 is set to 0%, how does it affect the response?
Category : 

Answer

Since the lower limit has been internally set, the setting value of 3 % or less is recognized as 3%.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800