• No : 21016
  • Release Date : 2018/08/22 16:25
  • Print

Gain adjustment under the speed control

What happens with the response when Pr.820 is set to 0%?
Category : 

Answer

Since the lower limit has been internally set, 3% or less is recognized as 3%.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800