• No : 21053
  • Release Date : 2018/08/22 16:25
  • Print

Safety stop function

There are connection diagrams that the safety relay module is connected to the multiple inverters. How many inverters can be connected to the safety relay module?
Category : 

Answer

Up to three inverters can be connected. When more than four inverters are connected, the inverters may not be recognized because of the voltage drop.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800