• No : 21085
  • Release Date : 2018/08/22 16:25
  • Print

Auto tuning

Is the capacity of the motor that can be handled by auto tuning the same as or one rank lower similarly to the A700?
Category : 

Answer

The 800 series supports the multiple rating. Thus, the rated current of the corresponding motor is 40% or higher of the inverter rated current. (Using a motor with the rated current substantially lower than the rated inverter current will cause torque ripples, etc. and degrade the speed and torque accuracies.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800