• No : 21102
  • Release Date : 2018/08/22 16:25
  • Print

PLC function

Can the PLC function be set without FR Configurator2?
Category : 

Answer

No. To set the PLC function, FR Configurator2 is required. (However, the setting cannot be configured with the trial version.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800