- No : 21142
- Release Date : 2018/08/22 16:26
-
Print
CC-Link
The inverter is driven with a programmable controller by using CC-Link. I want to reset the inverter when an error occurs due to overload, but it does not reset even the corresponding bit (RYB) is turned on. What should be done?
- Category :
-
Answer
The corresponding bit (RYB) can be used when a function other than reset is assigned to the RES terminal, but it cannot be used as the reset function. Use RY1A to reset the inverter. For the details, refer to "4.5 Inverter Reset" in the Instruction Manual of the FR-A7NC.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option