• No : 21145
  • Release Date : 2018/08/22 16:26
  • Print

FR-HC2

What is the measurement method and accuracy of the input current monitor?
Category : 

Answer

Three phases are measured with the CT. The accuracy is ±10 % which is same as the inverter output current.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
Option