- No : 21188
- Release Date : 2018/08/22 16:26
-
Print
Electronic bypass function
The Instruction Manual includes the following descriptions: "When connecting a DC power supply, insert a protective diode". Why is that?
- Category :
-
Answer
For countermeasures against the open/close surge of the MC (magnetic contactor). Insert a diode not to apply 27 VDC or more to the open collector terminal of the inverter due to surge.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700