• No : 21244
  • Release Date : 2018/08/22 16:26
  • Print

Model selection

When driving the motor of 132 kW/400 V under Advanced magnetic flux vector control, which inverter model should I use?
Category : 

Answer

Use the FR-A740. Basically, select the capacity according to the calculation result of "rated inverter output current ? rated motor current × 1.1".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700