• No : 21257
  • Release Date : 2018/08/22 16:26
  • Print

AM terminal output

Using two inverters, I want to use the voltage signal from the terminal AM of the first inverter as speed command of the second inverter. And also I want to set the output of terminal AM to 10 VDC when the first inverter operates at 70 Hz. How should I configure the setting?
Category : 

Answer

Set Pr.55 (Frequency monitoring reference) of the first inverter to 70 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700