• No : 21290
  • Release Date : 2018/08/22 16:26
  • Print

Installation of options

Which option should be installed to the inverter to output analog voltage 0 to 10 VDC?
Category : 

Answer

Use the digital output/additional analog output FR-A7AY (E kit).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700