• No : 21346
  • Release Date : 2018/08/22 16:27
  • Print

Frequency setting

I want to change the output frequency using CC-Link. Is it changed by changing the setting of Pr.1 (Maximum frequency)?
Category : 

Answer

Even though the maximum frequency setting is changed using CC-Link, the running frequency is not changed.
By writing the set frequency to the remote register RWw1 and turning ON RYD or RYE, the frequency setting completion turns ON and the frequency is set. (Set the frequency in units of 0.01 Hz.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700