- No : 21583
- Release Date : 2018/08/22 16:28
-
Print
Can I input speed setting externally with the box type?
Can I input speed setting externally with the box type?
- Category :
-
Answer
No.
Use the potentiometer on the box to set the speed. If you want to input analog values externally to set the speed, use the unit (module) type.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter speed controller
- Series
- SC-A