- No : 21607
- Release Date : 2018/08/22 16:28
-
Print
Range of carrier frequency
How wide is the carrier frequency range?
- Category :
-
Answer
You can vary the carrier frequency within the range of 0.7 to 14.5 kHz, and it is initially set to 1 kHz that generates low noise and leakage current.
You can change the carrier frequency by Pr.72 (PWM frequency selection).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024